:MEASure:TDEC:HWIDth
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEC:HWIDth <unit_interval>
<unit_interval> is a double.
Query Syntax
:MEASure:TDEC:HWIDth?
Description
Sets the width of the histograms used to configure a TDEC measurement (:MEASure:EYE:TDEC command) or VECP measurement (:MEASure:EYE:VECP command). The default value is 0.04 UI, which is the same value used in 100GBASE-SR4. The width setting can range from 0.01 UI to 0.20 UI. This command is equivalent to the TDEC/VECP Histogram Width setting which is located in the TDEC tab of the Configure Measurements dialog.
| Minimum Width (0.01 UI) | Maximum Width (0.20 UI) |
|---|---|
| TDEC Measurement (four histogram windows) | |
|
|
| VECP Measurement (two histogram windows) | |
|
|
Requires FlexDCA revision A.05.00 and above.