:MEASure:TDEC:LMLength
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEC:LMLength <number of ones>
<number of ones> is an integer from 2 to 1,024.
Query Syntax
:MEASure:TDEC:LMLength?
Description
Enters the level measurement length in UI for measuring TDEC. The length can range from 2 UI to 1,024 UI depending on these settings. The level measurement length must fit within the specified minimum allowed level runs:
- Minimum Zero Level Run:
:MEASure:TDEC:MRUN:ZEROcommand - Minimum One Level Run:
:MEASure:TDEC:MRUN:ONEcommand
This command is equivalent to the Level Measurement Length setting which is located in the Configure Measurements dialog's TDEC/VECP tab.
Requires FlexDCA revision A.07.60 and above.