:MEASure:TDEC:PRESets:SELections?
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:TDEC:PRESets:SELections?
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the TDEC (Transmitter and Dispersion Eye Closure) measurement. Use the PRESet command to load one of these presets.
TDEC Measurement Presets
- 400G CWDM8 MSA 10km Optical Interface
- IEEE 802.3bm (100 GbEn)
- ITU 50G PON
- Stressed Eye Closure (SEC)
- T11 FC-PI-6P (32xFibre Channel)
Requires FlexDCA revision A.05.00 and above.