:MEASure:TDEC:OLNGain
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEC:OLNGain <gain>
<gain> is a double between 1.000 and 12.000.
Query Syntax
:MEASure:TDEC:OLNGain?
Description
Sets the TDEC measurement's One Level Noise Gain which affects TDEC and VECP measurements. The default value is 1.000 and the range is 1.000 to 12.000.
Requires FlexDCA revision A.06.90 and above.