:MEASure:TDEC:MPNFactor
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEC:MPNFactor <noise_factor>
<noise_factor> is a double.
Query Syntax
:MEASure:TDEC:MPNFactor?
Description
Enters the mode partition noise factor for the TDEC measurement (:MEASure:EYE:TDEC command). This factor represents the mode partition noise contributed by the fiber-optic link that is connected to the output of the optical transmitter DUT. The default setting is 4.0 x 10−2. The range of values can be from 1 x 10−6 to 5 x 10−1. This command is equivalent to the Mode Partition Noise Factor setting which is located in the TDEC tab of the Configure Measurements dialog.
Requires FlexDCA revision A.05.00 and above.