:MEASure:TDEC:RHTime
Meas. mode:
Eye
Compatible waveforms:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEC:RHTime <double>
Where <double> is the position in UI (unit interval).
Query Syntax
:MEASure:TDEC:RHTime?
Description
Sets the position in UI (unit interval) of the right of two measurement histogram windows for a :MEASure:EYE:TDEC measurement. To position the left histogram window, use the :MEASure:TDEC:LHTime command.
This command is equivalent to the Right Histogram Position setting which is located in the TDEC/VECP configuration tab of the Configure Measurements dialog. To watch how the histogram changes while you adjust this setting, display the histograms on the waveform.
| Setting | Range | Default Value |
|---|---|---|
| Left Histogram Position | 0.25 to 0.50 UI | 0.4 UI |
| Right Histogram Position | 0.50 to 0.75 UI | 0.6 UI |
Requires FlexDCA revision A.05.80 and above.