:MEASure:TDEC:LHTime
Meas. mode:
                                                Eye
                                            Compatible waveforms:
                                                NRZ
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Command Syntax
:MEASure:TDEC:LHTime <double>
Where <double> is the position in UI (unit interval).
Query Syntax
:MEASure:TDEC:LHTime?
Description
Sets the position in UI (unit interval) of the left of two measurement histogram windows for a :MEASure:EYE:TDEC measurement. To position the right histogram window, use the :MEASure:TDEC:RHTime command.
This command is equivalent to the Left Histogram Position setting which is located in the TDEC/VECP configuration tab of the Configure Measurements dialog. To watch how the histogram changes while you adjust this setting, display the histograms on the waveform.
| Setting | Range | Default Value | 
|---|---|---|
| Left Histogram Position | 0.25 to 0.50 UI | 0.4 UI | 
| Right Histogram Position | 0.50 to 0.75 UI | 0.6 UI | 
Requires FlexDCA revision A.05.80 and above.