:SPRocess:RANDom:NOISe:BANDwidth
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RANDom:NOISe:BANDwidth <bandwidth>
<bandwidth> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:NOISe:BANDwidth?
Description
Use to specify a 3 dB response bandwidth when the :SPRocess:RANDom:NOISe:BANDwidth:AUTo command is set to a Gaussian response (automatic noise BW tracking of the input spectrum is turned off). These commands have no effect unless the random noise spectrum is selected to be bandwidth limited (:SPRocess:RANDom:NOISe:SPECtrum command).
Requires FlexDCA revision A.06.60 and above.