:SPRocess:RANDom:NOISe:RMS
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RANDom:NOISe:RMS <noise magnitude>
<noise magnitude> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:NOISe:RMS?
Description
Specifies the amount of random noise, in volts or Watts, applied by a Random operator. Use this command when the random noise spectrum is set to White noise (:SPRocess:RANDom:NOISe:SPECtrum) or Bandwidth limited noise (:SPRocess:RANDom:NOISe:SPECtrum) when the units are set to RMS (:SPRocess:RANDom:NOISe:UNITs).
Requires FlexDCA revision A.06.60 and above.
This command is equivalent to (but replaces) deprecated command :SPROcess:RANDom:NOISe.