:SPRocess:RANDom:NOISe:BANDwidth:AUTo
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RANDom:NOISe:BANDwidth:AUTo {ON | OFF}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:NOISe:BANDwidth:AUTo?
Description
Specifies that the bandwidth of the random noise added by the Random operator automatically tracks the input spectrum or has a Gaussian response. Before this command can take affect, you must select bandwidth limited random noise spectrum using the :SPRocess:RANDom:NOISe:SPECtrum command. If the random noise spectrum is set to white noise, this command has no effect.
- ON
- Noise BW automatically tracks input spectrum.
- OFF
- Noise BW has a Gaussian response.
Requires FlexDCA revision A.06.60 and above.