:SPRocess:RANDom:NOISe:UNITs
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RANDom:NOISe:UNITs {SDENsity | RMS)
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:NOISe:UNITs?
Description
When the random noise is set to be bandwidth limited (:SPRocess:RANDom:NOISe:SPECtrum), sets the units to be RMS (RMS) or spectral density (SDENsity). If RMS is specified, use the :SPRocess:RANDom:NOISe:RMS command to specify RMS magnitude. If SDENsity is specified, use the :SPRocess:RANDom:NOISe:SDENsity command to specify spectral density (η0).
Requires FlexDCA revision A.06.60 and above.