:SPRocess:RANDom:PRESets
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:SPRocess:RANDom:PRESets <string>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Loads a previously saved a preset for a Random Jitter/Noise operator. The preset configures the operator to your saved settings. To query which presets are available for loading, use the :RANDom:PRESets:SELections? query.
Random Operator Presets
- IEEE 802.3ck
Presets can only be saved from the operator's Setup dialog. There is no programming command for this task.
Requires FlexDCA revision A.06.60 and above.
Example Command
:SPRocess:RANDom:PRESets "MyPreset" // Load a saved preset.