:SPRocess:RANDom:PRESets:SELections
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Query Syntax
:SPRocessN:RANDom:PRESets:SELections?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the Random Jitter/Noise operator. Use the PRESet command to load one of these presets.
Random Operator Presets
- IEEE 802.3ck
Requires FlexDCA revision A.04.50 and above.