:SPRocess Subsystem
Use the :SPRocess
subsystem to select specific operator attributes for a Waveform Signal Processing operator.
The commands in this subsystem define the basic function. When you click on your function in Waveform Signal Processing Setup dialog, a setup dialog opens that allows you to configure your function. If a dialog does not appear, then there are no commands in the :SPRocess
that apply to the operator.
Operators are identified by their function assignment number (1 through 64) which is included in the SPRocess{1:64}
command. The following figure shows a Gaussian operator assigned to Function 1. Commands in this subsystem allow you to select the Gaussian operator's filter cutoff frequency. Before configuring an operator, assign the operator to a function using the :FUNCtion:FOPerator
command (:FUNCtion subsystem).
To create and configure a function:
- Use the
:FUNCtion:FOPerator
command (:FUNCtion subsystem) to create the function. - Use the commands in the
:SPRocess
subsystem to configure your function.
Common Display Setup Commands for Operators
The following commands are located in the :FUNCtion
Subsystem.