:TIMebase:MPOSition?
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Query Syntax
:TIMebase:MPOSition?
Description
Returns the minimum timebase position which is the minimum trigger delay setting. The minimum timebase position is for information only and cannot be changed. The set value depends on the oscilloscope that you are using:
- N1000A: 16 ns
- DCA-M: 10 ns
The minimum timebase position is displayed in the Trigger Setup dialog's Advanced Trigger Setup tab.
Starting with FlexDCA release A.08.30, the ability to set the minimum timebase position was removed. The query form of the command remains.