:TIMebase:SCALe
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:SCALe <seconds>
<seconds> is a double.
Query Syntax
:TIMebase:SCALe?
Description
Sets the horizontal timebase scale in seconds-per-division, when the timebase units are set to seconds (:TIMebase:UNITs). To change the timebase scale to symbols instead of seconds, use :TIMebase:UNITs. Use the :TIMebase:XLEFt? to query the time value at the graticule's left edge and :TIMebase:XRANge to set the time span across the graticule from the left edge to the right edge.
In Jitter Mode, perform an Auto Scale after changing this setting.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
Example Command Sequence
:TIMebase:UNITs SECond :TIMebase:SCALe 5.02E-12 :TIMebase:POSition 2.41E-08