:TIMebase:XRANge
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:XRANge <range>
<range> is a double.
Query Syntax
:TIMebase:XRANge?
Description
Sets or queries the full-scale horizontal time in seconds (span between the graticule left and right edges). Use :TIMebase:XLEFt? to query the time value at the graticule's left edge, :TIMebase:XRIGht? to query the time value at the graticule's right edge, and :TIMebase:SCALe to set the time-per-division setting.
In Jitter Mode, perform an Auto Scale after changing this setting.