:TIMebase:SRATe

Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter

Symbol Rate Selections

Availability of individual rates depends on installed modules and other conditions.

  • 51.84 MBd - STM-0/OC-1
  • 125.0 MBd - FDDI/100M Ethernet
  • 155.52 MBd - STM-1/OC-3
  • 270.0 MBd - SDI
  • 614.4 MBd - CPRI
  • 622.08 MBd - STM-4/OC-12
  • 768.00 MBd - OBSAI
  • 1.06250 GBd - 1G Fibre Channel
  • 1.22880 GBd - CPRI 2x
  • 1.244160 GBd - GPON/OC-24
  • 1.25000 GBd - Gb Ethernet
  • 1.48500 GBd - SDI
  • 1.50000 GBd - SATA-1/SAS-1
  • 1.53600 GBd - OBSAI 2x
  • 2.12500 GBd - 2B Fibre Channel
  • 2.4576 GBd - CPRI 4x
  • 2.48832 GBd - STM-16/OC-48
  • 2.50000 GBd - PCIe1/2 Gb Ethernet/InfiniBand
  • 2.6660570 GBd - STM-16/OC-48 FEC
  • 2.97000 GBd - SDI
  • 3.00000 GBd - SATA-2/SAS-2
  • 3.07200 GBd - CPRI 5x / OBSAI 4x
  • 3.12500 GBd - XAUI / 10GbE Base-LX4
  • 3.18750 GBd - FC-3187/10GBE Base-LX4
  • 3.25000 GBd - Rapid IO
  • 3.32000 GBd - 12x Parallel Optics
  • 4.25000 GBd - 4G Fibre Channel
  • 4.9152 GBd - CPRI 8x
  • 5.00000GBd - PCIe-2/2x InfiniBand
  • 6.00000 GBd - SATA-3/SAS3/CEI
  • 6.144 GBd - CPRI 10X / OBSAI 8X
  • 6.25000 GBd - 2x XAUI
  • 6.37500 GBd - CEI 6G+
  • 8.00000 GBd - PCIe-3
  • 8.1100800 GBd - CPRI 16x
  • 8.50000 GBd - 8x Fibre Channel
  • 9.8304 GBd - CPRI 16x
  • 9.95328 GBd - STM-64/OC-192/10GbEthernet
  • 10.00 GBd - InfiniBand QDR
  • 10.1376 GBd - CPRI 20x
  • 10.3125 GBd - 10Gb Ethernet LR/ER
  • 10.51875 GBd - 10G Fibre Chanel
  • 10.664230 GBd - STM-64/OC-192 FEC
  • 10.7090 GBd - STM-64/OC-192 FEC
  • 11.0000 GBd - CEI 11G
  • 11.0957 GBd - 10Gb Ethernet FEC
  • 11.3170 GBd - 10GFC FEC
  • 12.165120 GBd - CPRI 24x
  • 12.249450 GBd - STM-64/OC-192 SuperFEC
  • 12.44160000 GBd - ITU-T PON
  • 14.025000 GBd - 16G Fibre Channel
  • 14.06250 GBd - InfiniBand FDR
  • 16.00000 GBd - PCIe-4
  • 24.33024000 GBd - CPRI 48x
  • 24.88320000 GBd - ITU-T PON
  • 25.78125 GBd - 100GbE/4 / InfiniBand EDR
  • 26.56250000 GBd - 400GBASE-SR16
  • 27.7393 GBd - 100Gb Ethernet / 4 FEC
  • 27.952493 GBd - OTU4/ITU-T G.959.1
  • 28.05 GBd - 32G Fibre Channel
  • 28.9 GBd - 64G Fibre Channel
  • 32.00000 GBd - PCIe-5/PCIe-6
  • 39.81312 GBd - STM-256/OC-768
  • 41.250000 GBd - 40Gb Ethernet
  • 43.018413 GBd - STM-256/OC-768 FEC
  • 49.76640000 GBd - ITU-T PON
  • 53.125 GBd - 400GBASE
  • 56.100000 GBd - 128G Fibre Channel
  • 79.626240 GBd - STM-512/OC-1536
  • 106.25000 GBd - 800GBASE
  • 112.50000 GBd - 4x200G-FR4
  • 113.34570 GBd - 800GBASE (FECi)
  • 115.10417 GBd -
  • 159.25248 GBd - STM-1024/OC-3072

Command Syntax

:TIMebase:SRATe  <symbol rate>

<symbol rate> is a double.

Query Syntax

:TIMebase:SRATe?

Description

Enters the symbol rate used when the timebase units are set to unit interval (:TIMebase:UNITs). The following table shows some standard data rates. For example, for the CPRI 8x standard, you would enter:

:TIMebase:SRATe 4.9152E9

Setting the symbol rate automatically sets the unit-interval range :TIMebase:UIRange and unit-interval delay :TIMebase:UIPosition. To change the timebase scale to seconds instead of symbols, use :TIMebase:UNITs.

In Jitter Mode, symbol rate, symbols displayed, and symbol delay controls are disabled. Do not use this command in Jitter Mode. It generates an error.

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :TIMebase:BRATe.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.

Example Command Sequence

:TIMebase:UNITs UINTerval
:TIMebase:SRATe 9.953E+9