:TIMebase:UIPosition
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:UIPosition <UI delay>
<UI delay> is a double.
Query Syntax
:TIMebase:UIPosition?
Description
Sets the unit interval (UI) delay when the timebase units are set to unit interval (UI) (:TIMebase:UNITs). Use :TIMebase:UIRange to set the number of UIs displayed. Use :TIMebase:SRATe to automatically set the symbols displayed and UI delay based on the symbol rate.
In Jitter Mode, symbol rate, symbols displayed, and symbol delay controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :TIMebase:BPOSition.
Example Command Sequence
:TIMebase:UNITs UINTerval :TIMebase:UIRange 5.0E-01 :TIMebase:UIPosition 2.39874E+02