:TIMebase:POSition
Command Syntax
:TIMebase:POSition <seconds>
<seconds> is a double.
Query Syntax
:TIMebase:POSition?
Description
Sets the time at the delay reference point. The reference point is located at the display's left side (default) or the right side, as selected by the :TIMebase:REFerence command. In TDR mode, the reference point can also be set to two divisions in from the left side, which only affects the standard Waveform content window.
The position time specified establishes the time interval between the trigger event and the delay reference point, when the timebase units are set to seconds (:TIMebase:UNITs). This is the delay between the time a trigger is received and when the data is actually sampled. The maximum setting depends on the time-per-division setting. The minimum value you can set the horizontal position to is 10 ns (N1000A) defined at the left edge of the display graticule.
In Jitter Mode, scale and position controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
Example Command Sequence
:TIMebase:UNITs SECond :TIMebase:SCALe 5.02E-12 :TIMebase:POSition 2.41E-08