:TIMebase:SCRecovery:DEMethod
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:SCRecovery:DEMethod {CCRossing | PCRossings}
Query Syntax
:TIMebase:SCRecovery:DEMethod?
Query Response
{CCR | PCR}
Description
Selects the edge detection method that is applied to the software clock recovery. You can select an edge detection of either Center Crossing (CCRossing) or PAM4 Crossings (PCRossings), which is the default setting.
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.