:TIMebase:SCRecovery:PLLoop:JTF:BANDwidth

Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter

Command Syntax

TIMebase:SCRecovery:PLLoop:JTF:BANDwidth <bandwidth>

<bandwidth> is a double.

Query Syntax

TIMebase:SCRecovery:PLLoop:JTF:BANDwidth?

Description

Defines the bandwidth of a first- or second-order PLL's Jitter Transfer Function (JTF). The following table shows the bandwidth settings for some standards. Use the :TIMebase:SCRecovery:PLLoop:OJTF:BANDwidth command to set the bandwidth of the Observed Jitter Transfer Function (OJTF).

Standard JTF Bandwidth Settings
Standard First-Order Loop Filter Second-Order Loop Filter
SAS 1.5 Gb/s 900.0 kHz 900.0 kHz
SAS-SSC 1.5 Gb/s — 2.328 MHz
SATA 1.5 Gb/s — 4.097 MHz
SAS 3.0 Gb/s 1.800 MHz 1.800 MHz
SAS-SSC 3.0 Gb/s — 3.291 MHz
SATA 3.0 Gb/s — 1.791 MHz
SAS 6.0 Gb/s 3.600 MHz 3.600 MHz
SAS-SSC 6.0 Gb/s — 4.655 MHz
SATA 6.0 Gb/s — 8.194 MHz
QPI — 5.692 MHz
USB 3.0 — 10.03 MHz

This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.

Requires FlexDCA revision A.06.70 and above.