:TIMebase:SCRecovery:PLLoop:ORDer
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
TIMebase:SCRecovery:PLLoop:ORDer {FIRSt | SECond | THIRd}
Query Syntax
TIMebase:SCRecovery:PLLoop:ORDer?
Query Response
{FIRS | SEC | THIR}
Description
Selects a first, second, or third order low-pass filter for the FlexRT software clock recovery's phase lock loop. The following arguments are used:
- FIRSt
- Selects a first-order loop. Use the
:TIMebase:SCRecovery:PLLoop:MODEcommand to define either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) type of PLL. The transfer functions are defined using the:TIMebase:SCRecovery:PLLoop:JTF:BANDwidthand:TIMebase:SCRecovery:PLLoop:OJTF:BANDwidthcommands. - SECond
- Selects a second-order loop. This is the default selection. Use the
:TIMebase:SCRecovery:PLLoop:MODEcommand to define either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) type of PLL. The JTF is defined using the:TIMebase:SCRecovery:PLLoop:JTF:BANDwidthand:TIMebase:SCRecovery:PLLoop:JTF:PEAKingcommands. The OJTF is defined using the:TIMebase:SCRecovery:PLLoop:OJTF:BANDwidthand:TIMebase:SCRecovery:PLLoop:OJTF:DFACtorcommands. - THIRd
- Selects a third-order loop. Use the
:TIMebase:SCRecovery:PLLoop:FGAIncommand to enter the frequency for the loop's gain. Use the:TIMebase:SCRecovery:PLLoop:FPOLecommand to enter the frequency for the loop's pole. Use the:TIMebase:SCRecovery:PLLoop:FZERocommand to enter the frequency for the loop's zero.
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.