:TIMebase:SCRecovery:PLLoop:MODE
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
TIMebase:SCRecovery:PLLoop:MODE {JTF | OJTF}
Query Syntax
TIMebase:SCRecovery:PLLoop:MODE?
Query Response
{JTF | OJTF}
Description
Defines either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) for first- or second-order PLL loops. To select the loop order, use the :TIMebase:SCRecovery:PLLoop:ORDER command.
- JTF
- Specify the loop bandwidth with the
:TIMebase:SCRecovery:PLLoop:JTF:BANDwidthcommand. For second-order loops, define the loop peaking using the:TIMebase:SCRecovery:PLLoop:JTF:PEAKingcommand. - OJTF
- Specify the loop bandwidth with the
:TIMebase:SCRecovery:PLLoop:OJTF:BANDwidthcommand. For second-order loops, define the loop damping factor using the:TIMebase:SCRecovery:PLLoop:OJTF:DFACtorcommand.
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.