:TIMebase:SCRecovery:PLLoop:FZERo
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
TIMebase:SCRecovery:PLLoop:FZERo <frequency>
<frequency> is a double.
Query Syntax
TIMebase:SCRecovery:PLLoop:FZERo?
Description
For a third-order PLL loop, sets the frequency at which the OJTF starts to roll-off at 40 dB/decade. To set the frequency at which the JTF starts to roll-off at 40 dB/decade, use the :TIMebase:SCRecovery:PLLoop:FPOLe command. To enter the frequency that sets the approximate loop bandwidth of the PLL, use the :TIMebase:SCRecovery:PLLoop:FGAIn command. To select a third-order PLL loop, use the :TIMebase:SCRecovery:PLLoop:ORDer command.
with Zero, Pole, and Gain Frequencies
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.