Source Filter Setup

Instrument
AWG
N1000A
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
NRZ
PAM4

AWG Filter Setup

Use the Configure Source Filter for AWG dialog to add filtering to an AWG channel Data waveform. The following Filter Types can be selected. Enter a Filter Bandwidth for the selected filter.

  • 4th order Bessel
  • 1st order Butterworth
  • 2nd order Butterworth
  • 3rd order Butterworth
  • 4th order Butterworth
  • Gaussian
  • Sin(x)/x

The dialog is only available for channels that are defined as Data. Filtering can not be added to Clock waveforms.