Source Jitter & Noise Setup

Instrument
AWG
N1000A
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
NRZ
PAM4

AWG Jitter & Noise Setup

Use the Jitter & Noise for AWG Channel Setup dialog to apply a F/2 (Pk-Pk) jitter to an AWG channel Data waveform.

The dialog is only available for channels that are defined as Data. Jitter can not be added to Clock waveforms.