Screen/Pen/Touch Calibration
Screen/Pen/Touch calibration aligns the XY positions on touchscreen or mouse with the a display. The N1000A does not provide its own calibration application. Instead, exit the FlexDCA graphic interface and use the Windows start menu to search on "screen calibrate" or "touch" to locate the calibration application. If you have installed a custom mouse or pen pad, the manufacturer of the device may provide its own calibration application.