Sigma-E (rms) Result
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Sigma-E (rms) provides additional insight into the Signal-to-Noise-and-Distortion Ratio (SNDR) measurement. The SNDR measurement calculates the Sigma-E (rms) which is the standard deviation of error (distortion). Whenever you turn on the SNDR measurement, the Sigma-E measurement is automatically displayed as well as the Sigma-N (rms) measurement, and the P-Max or P-Signal measurement.
SCPI Command
:MEASure:PLEVel:SERRor