Level Results

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Meas. panel:
Jitter
Eye

Measures the amplitude for eye levels 0 and 1 for NRZ signals and levels 0, 1, 2, and 3 for PAM4 signals. You can modify the level measurement algorithm by clicking Measure > Configure Jitter Mode Measurements to open the Setup dialog. Select theAmplitude Measurements tab.Locate the Symbol Level Definitions and select either Average (the default value) or Consecutive Identical Digits.

NRZ Waveform
PAM4 Waveform

SCPI Command

:MEASure:AMPLitude:LEVel