DDJ (p-p) Result
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Meas. panel:
Jitter
Eye
The Jitter mode Data Dependent jitter (DDJ) measurements is pattern-related jitter caused by the combined effects of Inter-Symbol Interference (ISI) and Duty Cycle Distortion (DCD). In Jitter Mode, Data Dependent Jitter is the peak-to-peak spread of the histogram of all edges as shown in the DDJ Histogram graph.
More Information
SCPI Command
:MEASure:JITTer:DDJ