UJ (rms) Result)
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Click the Measurement (Meas) toolbar's UJ to activate Jitter mode's Uncorrelated Jitter (UJ) measurement which is the total of the following values:
- Random Jitter (RJ) that is unpredictable and not data related, and
- Asynchronous Periodic Jitter (APJ) that is periodic jitter that is uncorrelated to the symbol rate.
The relationship of UJ is shown in the Jitter Components Tree.
More Information
SCPI Command
:MEASure:JITTer:UJ