Measurement Levels Results

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Measures the jitter sampling level, which is the amplitude at which jitter measurements are made. Jitter sampling level is specified as a percentage, custom, or average value in the Thresholds tab of the Jitter Mode Measurement Setup dialog.

This measurement can only be viewed in the results panel by sending the :MEASure:JITTer:LEVel command.

More Information

SCPI Command

:MEASure:JITTer:LEVel