Impedance Setup

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

The Transmitter and Receiver Impedance Setup dialogs are displayed whenever you click on the impedance symbol in your network setup diagram. Use this dialog to enter the impedance values for both the Measurement and Simulation circuits. Select Use Single Impedance Value to force one value to define both circuits. The default impedance value is 50 ohms.