Differential DeEmbedding Operator

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

The Differential De-Embedding operator provides the most precision for removing or inserting test-setup elements. Click on these operator to create a network that describes the full system of transmitter, receiver, and channel blocks. For each block, both measurement and simulation electrical circuits are defined. The measurement circuit models the actual physical electrical circuit that produced the measured waveform. The simulation circuit models a hypothetical electrical circuit that exhibits the characteristics that you want to measure.

The operator's Display Setup configures the manner in which the resulting waveform is displayed including both vertical and horizontal scaling. For more information, refer to Common Display Settings.

De-Embedding Network File

Click to Create a New Network to define your de-embedding network. Your network setups are saved in files.

Click if you have already configured and saved a network file. The selected network file is loaded for use. After opening a network file, click Edit the Selected Network to change the network's configuration.

In your definitions, you can enable the most complete waveform rendering by including the reflective S-parameter elements in the mathematical calculation of the correction transfer function file which is used to transfer data from the measurement to the simulated (displayed) measurement.

The default user data folder for de-embedding network files is \De-Embedding Networks.

Operator Output

Select the Operator Output to be: Differential, Common Mode, or Single-Ended.

Options

Use the Filter field to select a Gaussian Filter, Sinc Filter, or None for no filtering.

If needed, use the Bandwidth field to minimize effects caused by noise that occurs above the frequency where the signal is mostly attenuated. Normally the FlexDCA automatically sets the bandwidth limit. Or, manually enter a bandwidth from 10 MHz to 1 THz with a default value of 7.5 GHz.

You can set the operators Maximum Gain in the range of 0 dB to 100 dB. The default value is 20 dB.

Clear the Align Input and Output Waveforms field to view the delay introduced by your device. By default, this field is normally selected and the input and output waveforms are aligned.

Noise Processing

None Selection

The option None does not make any special considerations for aliased noise. This is an appropriate choice when the waveform is known to have no aliased components, such as from a real-time or simulated source. This also is the preferred choice when dealing with averaged waveforms where the desired outcome is to remove noise and interference components that are not correlated to the trigger signal.

Process Spectrum Selection

The option Process Spectrum works by applying the transfer function of the filter to the power spectrum of the noise to determine the appropriate magnitude of the noise on the output signal.

The default behavior of the Process Spectrum noise processing option is to use the noise power spectrum of the input signal. If the input signal is a sampling scope channel with SIRC active, this spectrum will be established by the measured hardware response of the channel. For other channels, the response will be assumed Gaussian with a 3 dB frequency corresponding to the nominal channel bandwidth. This behavior can be overridden by clearing the Track Input Response checkbox and manually entering a bandwidth. If this option is utilized the response will be presumed Gaussian with the selected 3 dB bandwidth.

Preserve RMS Selection

The option Preserve RMS is appropriate when the noise bandwidth is very low relative to the channel and filter bandwidth. It is also appropriate when the aliased components are known to have most of the power within a range of in-band frequencies. This could be from laser RIN, for example, or from intentionally modulated interference/crosstalk. When Preserve RMS is selected, the RMS magnitude of the aliased components will be scaled by the DC gain (the sum of the taps) of the filter. For the low-pass filters (Bessel, Butterworth, Gaussian, Sinc), the DC gain is unity. For the equalizers and embedding/de-embedding operators, the DC gain depends upon the settings of the operator.

By tracking the accumulated effects of the filtering operations, accurate noise processing can be done even when chaining operations as illustrated in the following figure. In addition to the sampled waveform, information about the acquisition channel and noise power spectrum are maintained in each signal and appropriately processed by each filter. The complete set of auxiliary information is also included when storing FlexDCA waveforms in the *.wfmx file format.

FlexDCA Waveform Processing

The noise processing feature was added in FlexDCA version A.06.60 and above.

These operators are not available in TDR/TDT mode.

These operators requires a single-valued waveform, as opposed to an eye diagram. Be sure that your trigger setup results in a single-valued waveform at the input to this operator. This can be acheived using an external pattern trigger or by using pattern lock. If you are using an external pattern trigger, you may ignore this note.

The convolution process used by this operator requires that the measurement circuit and the simulation circuit be linear and time-invariant (small-signal analysis requirements).