:TPRogram:SETup:ADD
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:ADD
Adds Test Program lines to a Station's Test Program. Each line defines a set of measurements for a specified fixture's lane and is configured using the remaining commands in the :TPRogram:SETup SCPI note. To run the Test Program, use the :TPRogram:RUN command.
To remove the last line in a Test Program, use the :TPRogram:SLINe:REMove command. To remove all Test Program lines, :TPRogram:CLEar command.