:TPRogram:SETup:THRatio

Flex Apps:
FlexOTO
FlexOTO Instance:
Stations

Command Syntax

:TPRogram:SETup:THRatio <hit_ratio>

<hit_ratio> is a double.

Description

For the Test Plan, selects the Target Hit Ratio for the overshoot and undershoot measurements. The default hit ratio is 0.01 which is called out in the IEEE 802.3cu standard. The minimum value is 0.0. The maximum value is 0.1.

To change the Target Hit Ratio for a single line in the Test Program, use the :TPRogram:SLINe:THRatio command.

Measurements Affected by Configuration Settings (PAM4 Waveform)
Measurement Power Units Outer ER Units Linearity Definition Target Transition Target Hit Ratio
:TPRogram:SETup:PUNits :TPRogram:SETup:ERUNits :TPRogram:SETup:LDEFinition :TPRogram:SETup:TRANsition :TPRogram:SETup:THRatio
Average Power ■
Ceq Noise Gain
Levels ■
Linearity ■
Outer ER ■
Outer OMA ■
Overshoot ■
Peak-Peak Power ■
TDECQ
Transition Time ■
Tx Power Excursion ■ ■
Undershoot ■