:TPRogram:SETup:EDIMage:SRESults
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:EDIMage:SRESults {ON | OFF}
Query Response
{0 | 1}
Description
When adding new lines to a Test Program, specifies whether the measurements results will be rasterized and embedded as part of the eye diagram image. The default setting is ON. In addition to setting this command, be sure to select that an image be saved by appending the EDIMage argument to the :TPRogram:SLINe:MEASurements command.