:TPRogram:SETup:FIXTure:ALL
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:FIXTure:ALL {DISabled | ENABled}
Description
When adding new lines to a Test Program, enables or disables all lanes and all fixtures for measurements. To enable or disable individual lanes for a specified fixture, use the :TPRogram:SETup:FIXTure parent command. The :TPRogram:SETup:FIXTure:ALL command is equivalent to the Fixture Lanes settings field in the Test Program Measurement Setup dialog.
If your Station has multiple Fixtures, and you want to disable all of the lanes on a particular Fixture, send the :TPRogram:SETup:FIXTure command without any lane arguments.