:TPRogram:SETup:EDIMage:UWBackground
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:EDIMage:UWBackground {ON | OFF}
Query Response
{0 | 1}
Description
When adding new lines to a Test Program, sets an image's background to white (default is black) when an eye diagram is saved to an image file.
ON- Select a white background. This setting is ideal for images that are going to be printed or included in a PDF. A white background maked the image easier to see and used less printer toner.
OFF(default setting)- The default black background is used on the image.
To specify that an image be saved with the measurement results, add the EDIMage argument to the :TPRogram:SETup:MEASurements command. The :TPRogram:SETup:EDIMage:UWBackground command is equivalent to the Use White Background field in the Test Program Measurement Setup dialog.
When editing existing lines in a Test Program, use the :TPRogram:SLINe:EDIMage:UWBackground command.