:TPRogram:SETup:EDIMage:IMETadata
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:EDIMage:IMETadata {ON | OFF}
Query Response
{0 | 1}
Description
When adding new lines to a Test Program, embeds metadata into an image when an eye diagram is saved to a JPEG or TIFF image file. The command is equivalent to the Include Metadata field in the Test Program Measurement Setup dialog. This setting is on by default.
To specify that an image be saved with the measurement results, add the EDIMage argument to the :TPRogram:SETup:MEASurements command. To specify that a JPEG or TIFF file is saved, use the :TPRogram:SLINe:EDIMage:FTYPe command.
The metadata data that is embedded includes information such as:
- CreatorTool: "FlexOTO (P.07.XX.XXX)"
- CreateDate: "2023-09-21T10:07:20"
- Make: "Keysight Technologies"
- Model: "FlexOTO (P.07.XX.XXX)"