:WMEMory:CWINdow

Command Syntax

:WMEMoryN:CWINdow TIME{1:4}

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:CWINdow?

Description

The :WMEMory{1:8}:CWINdow command selects a content window in which to display a waveform memory waveform.

Command Arguments and Content Windows
Argument Displayed Waveform
Content Window
Number of
Available Windows
Scale Units
Programmatically Via
Front Panel
TIME{1:4} Waveform 4 4 Y-Axis: Volts or Watts (linear scale)
X-Axis: seconds