:WMEMory:DSTatus:DETails?
Query Syntax
:WMEMoryN:DSTatus:DETails?
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Response
<string>
Description
If the status of the specified waveform memory is invalid (see :WMEMory:DSTatus?), this query returns a string that may provide additional details.
If the status of the specified waveform memory is valid, this query returns an empty string.
For a basic reason for the invalid status, use the :WMEMory:DSTatus:REASon? sibling query.