:WMEMory:INTerpolate:STATus:DETails?

Query Syntax

:WMEMoryN:INTerpolate:STATus:DETails?

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Response

<string>

Description

If the status of the specified waveform memory's interpolation on load is invalid (see :WMEMory:INTerpolate:STATus?), this query returns a string that may provide additional details.

If the status of the specified waveform memory interpolation on load is correct, this query returns an empty string.

For a basic reason for the questionable or invalid status, use the :WMEMory:INTerpolate:STATus:REASon? sibling query.