:WMEMory:UNAMe:UFName

Command Syntax

:WMEMoryN:UNAMe:UFName

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Description

Automatically sets the waveform memory's user name to the name of the waveform's source file. If the waveform was loaded from a displayed input channel, the name of the file that was automatically created when the data was loaded is used. To learn about user names, use the default user name, or enter a custom user name, use the :WMEMory:UNAMe command.