:WMEMory:PATTern:INVert
Command Syntax
:WMEMoryN:PATTern:INVert {{ON | 1} | {OFF | 0}}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:PATTern:INVert?
Query Response
{1 | 0}
Description
When detecting a known pattern or a pattern that is loaded from a file (see :WMEMory:PATTern:MODE), this command lets you detect an inverted version of the known or loaded pattern.