:WMEMory:PATTern:FILE:RELoad

Command Syntax

:WMEMoryN:PATTern:FILE:RELoad

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Description

When you have specified a PAM signal type (see :WMEMory:SIGNal:TYPE) and specified the signal pattern by loading a pattern file (see :WMEMory:PATTern:FILE:NAME), this command reloads the specified pattern file. Reloading is useful when there have been changes to the pattern file that was previously loaded.