:WMEMory:PATTern:FILE:NAME

Command Syntax

:WMEMoryN:PATTern:FILE:NAME "filename"

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:PATTern:FILE:NAME?

Query Response

"string"

Description

When you have chosen "loading a pattern file" to identify the data signal pattern (see :WMEMory:PATTern:MODE), this command lets you specify the name of the file to load. The file name is a quoted full-path string.

If there are changes to the pattern file that has been loaded, use the :WMEMory:PATTern:FILE:RELoad command.