:WMEMory:DSTatus?

Query Syntax

:WMEMoryN:DSTatus?

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Response

{CORR | INV}

Description

Returns the status of the specified waveform memory. Up to eight memories are available. To query the reason for the current state of the memory, use the :WMEMory:DSTatus:REASon? query. The following responses can be returned:

CORR
The memory location contains waveform data. To clear memory, use the :WMEMory:CLEar command.
INV
The memory location does not contain waveform data.