:WMEMory:TTIMebase
Command Syntax
:WMEMoryN:TTIMebase {ON | OFF | 1 | 0}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:TTIMebase?
Query Response
{1 | 0}
Description
Turns the track timebase function on and off. With track timebase on, the time scale and position of the displayed waveform memory is set to and tracks the time scale and position settings made in the :TIMebase subsystem (:TIMebase:SCALe and :TIMebase:POSition).